Hardware requirements#
Micro USB cable
two IMX95VERDIN-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
Populate J57
Connection as below:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J57 pin 1 SCL J57 pin 1
SDA J57 pin 2 SDA J57 pin 2
GND J26 pin 2 GND J26 pin 2
Please note this application can’t support running with Linux BSP!
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch S6 to power on the board.
Connect a micro USB cable between the host PC and the J4 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board EDMA example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .