Hardware requirements#
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.