Hardware requirements#
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings#
connect input signal to J1-15
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the demo in the terminal window:
TPM dual-edge capture example
Once the input signal is received the input capture values are printed
The input signal's pulse width is calculated from the capture values & printed
Capture value C(n)V=11d5a52
Capture value C(n+1)V=11d5a60
Input signals pulse width=2 us