Hardware requirements

  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo

  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

These instructions are displayed/shown on the terminal window:

GPIO Driver example
The LED is blinking.

And you will detect voltage toggle on J2 Pin 1. If the LOC board is used then the blue led will blink.