MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings#

connect input signal to J1-1

Prepare the Demo#

  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the demo in the terminal window:

TPM dual-edge capture example

Once the input signal is received the input capture values are printed
The input signal's pulse width is calculated from the capture values & printed

Capture value C(n)V=11d5a52

Capture value C(n+1)V=11d5a60

Input signals pulse width=2 us