Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
You will see the welcome string printed out on the console. You can send characters to the console back and they will be printed out onto console in a group of 4 characters. Be aware of 10s RX timeout. User must provide input within timeout period, otherwise timeout expire.
FreeRTOS LPUART driver example.
aaaabbbbcccc