Hardware requirements#
Micro USB cable
LPC845 Breakout board
Personal Computer
Board settings#
PIO0_14 is ACOMP negative input pin, which can sample external voltage.
Prepare the demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the ACOMP interrupt driver example in the terminal window:
LPC_ACOMP Interrupt Example.
The example compares analog input to the voltage ladder output(ACOMP negative port).
The LED will be turned ON/OFF when the analog input is LOWER/HIGHER than the ladder's output.
Change the analog input voltage to see the LED status.