Hardware requirements#
Mini/micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
Pin P0_21 is used as a CLKOUT signal. Connect this pin to an Oscilloscope for viewing the signal.
Running the demo#
The demo sets the MicroTick Timer as a wake up source and puts the device in deep-sleep mode. The MicroTick timer wakes up the device. After wake up the Green LED on the board blinks and a CLKOUT signal can be seen on pin P0_21.