Hardware requirements#
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
USART RX ring buffer example
Send back received data
Echo every 8 bytes