MCUXpresso SDK Documentation

Hardware requirements

Hardware requirements#

  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings#

  1. Pin P3_12(j12-9) is used as a CLKOUT signal. Connect this pin to an Oscilloscope for viewing the signal.

Running the demo#

The demo sets the MicroTick Timer as a wake up source and puts the device in deep-sleep mode. The MicroTick timer wakes up the device. After wake up the LED3 on the board blinks and a CLKOUT signal can be seen on pin P3_12. The demo is not recommended to use debug mode In MCUXpresso, POWER_EnterDeepSleep () will kill the debug session.