Hardware requirements
Two micro USB cables
LPCLPCXpresso54628 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the +5V Power only USB port on the target board (J1).
Connect a USB cable between the host PC and the Debug Link USB port on the target board (J8).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the OTP demo in the terminal window:
OTP Peripheral Driver Example
OTP ROM API driver version: 0x101