MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings#

USART hardware flow control on one board. The USART sends data to itself(loopback), and hardware flow control function is enabled on this example. So please make sure the correct connection for example.

Pin Name    Board Location    connect to     Pin Name    Board Location
USART_TX    J13   Pin 13      ----------     USART_RX    J13   pin 15
USART_CTS   J13   Pin 16      ----------     USART_RTS   J13   Pin 14

Prepare the Demo#

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

This is USART hardware flow control example on one board.
This example will send data to itself and will use hardware flow control to avoid the overflow.
Please make sure you make the correct line connection. Basically, the connection is:
      USART_TX    --     USART_RX
      USART_RTS   --     USART_CTS
Data matched! Transfer successfully.