MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings#

No special is needed.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

USART RX ring buffer example
Send back received data
Echo every 8 bytes