Hardware requirements
Mini USB cable
LPCXpresso54628 board
Personal Computer
Board settings
Insert the card into the card slot
Prepare the Example
Connect a mini USB cable between the PC host and the OpenSDA USB port (J2) on twrk64f120m board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
FATFS example to demonstrate how to use FATFS with MMC card.
Make file system......The time may be long if the card capacity is big.
Create directory......
Create a file in that directory......
List the file in that directory......
General file : F_1.DAT.
Write/read file until encounters error......
Write to above created file.
Read from above created file.
Compare the read/write content.
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.