Hardware requirements#
Micro USB cable
LPCXpresso54S018M board
Personal Computer
Board settings#
ADC CH4 input signal J12-2(PIO0-16).
Prepare the Demo#
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018M.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Press any key from keyboard and trigger the conversion. The log below shows example output of the ADC basic example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
...