Hardware requirements
Mini/micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the PUF driver example in the terminal window (the key value will vary):
PUF Peripheral Driver Example
Reconstructed key = ad e7 b4 fe 99 ce 41 b7 c6 f9 78 2f 49 6b 87 27
Example end.