Hardware requirements#
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings#
Keep jumper JS3 open for proper SW4 button operation.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Use SW4 button to control blue and green LED and SW1 to control GPIO mask feature. If SW4 button is pressed (logical zero is read), the GREEN LED is switched on in secure world and blue LED is switched on from normal world. So both blue and green LEDs are controlled by SW4 button. If also SW1 button is pressed, the GPIO mask feature is activated. In this case the blue LED starts to light regardless of SW4 button state, since normal GPIO cannot read state of SW4 button (only the logic 0 is read). The green LED can be still controlled by SW4 button.
TrustZone Application Development in SDK#
Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.
The secure project is stored in <application_name><application_name>_s directory. The non-secure project is stored in <application_name><application_name>_ns directory.
The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. If IDE allows the two projects in single workspace, the user can also find the project with <application_name>. This project contains both secure and non-secure projects in one workspace (Keil MDK, IAR) and it allows to user easy transition from one to another project.
Project Structure#
The all TrustZone files related to TrustZone are located in trustzone virtual directory. The files are:
tzm_config.c
tzm_config.h
veneer_table.c
veneer_table.h
File tzm_config.c, tzm_config.h#
This file is used by secure project only. It contains one function BOARD_InitTrustZone(), which configures complete TrustZone environment. It includes SAU, MPU’s, AHB secure controller and some TrustZone related registers from System Control Block. This function is called from SystemInitHook() function, it means during system initialization.
File veneer_table.c, veneer_table.h#
This file defines all secure functions (secure entry functions) exported to normal world. This file is located in secure project only. While header file is used by both secure and non-secure projects. The secure entry functions usually contain validation of all input parameters in order to avoid any data leak from secure world.
The files veneer_table.h and <application_name>_s_import_lib.o or <application_name>_s_CMSE_lib.o create the connection between secure and non-secure projects. The library file is generated by linker during compilation of secure project and it is linked to the non-secure project as any other library.
TrustZone application compilation#
As first compile secure project since CMSE library is needed for compilation of non-secure project. After successful compilation of secure project, compile non-secure project.
TrustZone application debugging#
Download both output file into device memory
Start execution of secure project since secure project is going to be executed after device RESET.
If IDE (Keil MDK, IAR) allows to manage download both output files as single download, the secure project is configured to download both secure and non-secure output files so debugging can be fully managed from secure project.
Device header file and secure/non-secure access to the peripherals#
Both secure and non-secure project uses identical device header file. The access to secure and non-secure aliases for all peripherals is managed using compiler macro __ARM_FEATURE_CMSE.
For secure project using <PERIPH_BASE> means access through secure alias (address bit A28=1), using <PERIPH_BASE>_NS means access through non-secure alias(address bit A28=0) For non-secure project using <PERIPH_BASE> means access through non-secure alias (address bit A28=0). The non-secure project doesn’t have access to secure memory or peripherals regions so the secure access is not defined.