Hardware requirements#
Micro USB cable
LPCXpresso55S16 board
Personal Computer
Board settings#
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
DMA wrap transfer example begin.
Destination address wrap transfer:
5 6 7 8 0 0 0 0
Source address wrap transfer:
1 2 3 4 1 2 3 4
DMA wrap transfer example finish.