Hardware requirements

  • Micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings

Connect SPI7 pins to SPI2 pins:

    Master(SPI7)		           Slave(SPI2)
Pin Name   Board Location     Pin Name   Board Location
MISO       J9    pin 11       MISO       J12   pin 5
MOSI       J9    pin 9        MOSI       J12   pin 9
SCK        J9    pin 13       SCK        J12   pin 7
SSEL1      J9    pin 2        SSEL0      J12   pin 13

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.