Hardware requirements#
Mini USB cable
LPCXpresso55S28 board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
USART CMSIS interrupt example
Board receives 8 characters then sends them out
Now please input:
When you input 8 characters, system will echo it by USART and them would be seen on the OpenSDA terminal.