Hardware requirements
Mini USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Prepare the Demo
Connect a mini USB cable between the PC host and the LPC-Link USB port (J1) on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
The following message shows in the terminal if the example runs successfully.
USART CMSIS interrupt example
Board receives 8 characters then sends them out
Now please input:
When you input 8 characters, system will echo it by USART and them would be seen on the OpenSDA terminal.