Hardware requirements#
Micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the terminal like:
USART RX ring buffer example
Send back received data
Echo every 8 bytes