Hardware requirements#
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world demo in the terminal window:
* PSA crypto example *
cipher encrypt/decrypt AES CBC no padding:
success!
cipher encrypt/decrypt AES CBC PKCS7 multipart:
success!
cipher encrypt/decrypt AES CTR multipart:
success!
cipher encrypt/decrypt AES CBC no padding one go:
success!
cipher encrypt/decrypt AES CBC PKCS7 padding one go:
success!
Hash a message SHA-256:
success!
* Example End *