Hardware requirements#
Micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings#
Pin P19_2 is used as a CLKOUT signal. Connect this pin to an Oscilloscope for viewing the signal.
Running the demo#
The demo sets the MicroTick Timer as a wake up source and puts the device in sleep mode. The MicroTick timer wakes up the device.
After wake up:
(1)the red LED on the board blinking. (2)CLKOUT signal changing can be seen on pin P19_2.And the frequency of output signal will double.
If the demo run successfully, you will see the log from debug console:
Utick wakeup demo start...
Wakeup from sleep mode...