Hardware requirements

  • Mini/micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

The Multicore RPMsg-Lite pingpong RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

For detailed instructions, see the appropriate board User’s Guide.

Running the demo

The log below shows the output of the RPMsg-Lite pingpong RTOS demo in the terminal window:

RPMsg demo starts

Copy CORE1 image to address: 0x20033000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101

RPMsg demo ends

Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.