Hardware requirements#
LPCXpresso 55S69 board
Mini/micro USB cable
Personal Computer
Board settings#
No special HW settings are required.
In case of MCUBoot for LPC55S69 there is currently no image revert mechanism. This is due to Flash ECC capability that doesn’t allow incremental flash programming. MCUBoot’s revert strategies rely on this mechanism, therefore it’s not currently practical to use any of the MCUBoot’s revert strategies like image swapping by move or stratch area.
MCUBoot memory layout#
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x00000000 |
0x0001FFFF |
128kB |
Primary slot |
0x00020000 |
0x0004FFFF |
192kB |
Secondary slot |
0x00050000 |
0x0007FFFF |
192kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use its OVERWRITE_ONLY image handling strategy
To manually enter serial recovery mode during reset, keep button SW1 pressed
Image signing example#
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 4
--version 1.1
--slot-size 0x30000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
NOTE - there is alternative prj.conf file named prj-mbedtls.conf that can be used to enable mbedtls with HW crypto acceleration.