Hardware requirements
Micro USB cable
LPCXpresso54018 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
WKT interrupt example
Self-wake-up timer interrupt is occurred ! Self-wake-up timer interrupt is occurred ! Self-wake-up timer interrupt is occurred ! Self-wake-up timer interrupt is occurred ! Self-wake-up timer interrupt is occurred !
And the LD21&&LE22 will start to shine.