Functional description#
This example shows the usage of burst transfer from source buffer to destination buffer.
Hardware Requirements#
Mini/micro USB cable
LPCXpresso824MAX board
Personal Computer
Board Settings#
No special settings are required.
Run the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP port(J3 on the board).
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the
[Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).
Launch the debugger in your IDE to begin running the demo.
Expected Result#
When the example runs successfully, the following message is displayed in the terminal:
DMA wrap transfer example begin.
Destination address wrap transfer:
5 6 7 8 0 0 0 0
Source address wrap transfer:
1 2 3 4 1 2 3 4
DMA wrap transfer example finish.