Toolchain supported#
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements#
Micro USB cable
LPCXpresso54608 board
Personal Computer
Board settings#
ADC CH0 input signal J1-6(PIO0-7).
Prepare the Demo#
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world demo in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
...