Hardware requirements#
Micro USB cable
MC56F80000-EVK board
Personal Computer
Board hardware common setting#
Power setting:
Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2
Reset pin setting:
Connect J11 pin2 and pin3
Debugger setting:
Connect J13 pin 1-2, 3-4, 5-6, 7-8
Board settings#
Connect J17 pin 1-2.
Prepare the Demo#
Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with Multilink debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
These instructions are displayed/shown on the terminal window:
GPIO Driver example
Press the button SW2 to toggle the LED
Press the button SW2 and you will find the RED LED is toggled with log output.
Button press event detected....