Hardware requirements
Target microcontroller board
Personal Computer
FreeMASTER 2.5 or later installed on PC
Board settings
By default, the demo is configured for standard Serial (UART) communication. It may be changed to other interface in MCUXpresso SDK ConfigTools. Such other communication interfaces may require different physical connections made on board, such as CAN transceiver or direct MCU’s USB port. Refer to readme.txt files in other FreeMASTER demos which are available for this platform to see more details about board setup.
Prepare the demo
Interconnect the host PC and the target microcontroller board using the selected interface cable.
Compile and download the program to the target microcontroller.
Run and resume application execution when debugger stops in the main() function.
Connect with FreeMASTER
Run FreeMASTER, use the Connection Wizard or open Project Options.
Configure Serial, CAN or other communication as required by this demo setup.
Start communication, FreeMASTER loads the initial TSA Active Content links in the Welcome page.
Click the “FreeMASTER Demonstration Project (embedded in device)” in the Welcome page.
The demo is now running, you should be able to watch variable values and graphs.
More information
Read more information about FreeMASTER tool at http://www.nxp.com/freemaster. Feel free to ask questions and report issues at FreeMASTER’s community page at https://community.nxp.com/community/freemaster