Hardware requirements#
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Oscilloscope
Board settings#
CM33: connect J17-16(TPM2_CHN0), J17-29(GND) to Oscilloscope
CM33: connect J17-18(TPM2_CHN1), J17-29(GND) to Oscilloscope
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
TPM example to output combined complementary PWM signals on two channels
If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value: