Hardware requirements#
USB Type-C cable
two MCIMX93-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J1005 pin 3 SCL J1005 pin 3
SDA J1005 pin 5 SDA J1005 pin 5
GND J1005 pin 7 GND J1005 pin 7
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Boot Linux BSP to u-boot, and load M core image from SD card to run. (Put the image into SD card before.) => load mmc 1:1 0x80000000 /sdk20-app.bin => cp.b 0x80000000 0x201e0000 0x20000 => bootaux 0x1ffe0000 0
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board EDMA example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .