Hardware requirements#
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
USB to TTL converter
Board settings#
Connect the USB to TTL converter to MCX-N5XX-EVK board. MCX-N5XX-EVK UART pins: TX pin is connected with RX pin.
LPUART0 CONNECTS TO LPUART0
Pin Name Board Location Pin Name Board Location
TXD J20-9(P0_12) RXD J20-12(P0_13)
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
LPUART 9-bit mode example begins
LPUART is configured with 9bit
LPUART will send data out:
0x100 0x101 0x102 0x103 0x104 0x105 0x106 0x107
0x108 0x109 0x10a 0x10b 0x10c 0x10d 0x10e 0x10f
LPUART received data:
0x100 0x101 0x102 0x103 0x104 0x105 0x106 0x107
0x108 0x109 0x10a 0x10b 0x10c 0x10d 0x10e 0x10f
All data matches!