Hardware requirements
Micro USB cable
MCX-N5XX-EVK board
Personal Computer
3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A
Board settings
Attach the LCD shield to the EVK board.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
If this example runs correctly, the sample GUI is displayed.
Note
NOTE: Revision A0 chip can’t use SmartDMA for FlexIO display. Use the function
Chip_GetVersion to check silicon revision. For A0 chip, BOARD_USE_FLEXIO_SMARTDMA
must be set to 0, for A1 chip, BOARD_USE_FLEXIO_SMARTDMA can be set to 1
for better performance.