Hardware requirements

  • Micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

  • 3.5” TFT LCD module by NXP (P/N PAR-LCD-S035)

Board settings

Attach the LCD shield to the EVK board.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Build the project.

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

If this example runs correctly, the sample GUI is displayed.

Note

NOTE: Revision A0 chip can’t use SmartDMA for FlexIO display. Use the function Chip_GetVersion to check silicon revision. For A0 chip, BOARD_USE_FLEXIO_SMARTDMA must be set to 0, for A1 chip, BOARD_USE_FLEXIO_SMARTDMA can be set to 1 for better performance.