Hardware requirements#
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the demo in the terminal window:
TPM example for output compare
You will see the output signal toggle
Probe the signal using an oscilloscope
Use oscilloscope to measure output signal pin at J1-15.