Hardware requirements#
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world demo in the terminal window:
hello world.