Hardware requirements#
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings#
UART hardware flow control on one board. The UART will send data to itself(loopback), and hardware flow control function will be enabled on this example. So, please make sure the correct connection for example.
Pin Name Board Location connect to Pin Name Board Location
LPUART_TX J2 Pin 4 ---------- LPUART_RX J2 pin 3
LPUART_CTS J1 Pin 1 ---------- LPUART_RTS J2 Pin 1
Short the JP23-2 and JP23-3 with the jumper, other jumpers keep default configuration.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
This is LPUART hardware flow control example on one board.
This example will send data to itself and will use hardware flow control to avoid the overflow.
Please make sure you make the correct line connection. Basically, the connection is:
LPUART_TX -- LPUART_RX
LPUART_RTS -- LPUART_CTS
Data matched! Transfer successfully.