Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the eRPC Two Way RPC RTOS demo in the terminal window:
Primary core started
Get number from core1:
Got number: 1
Start normal rpc call example.
RPC call example finished.
Get number from core1:
Got number: 2
Start normal rpc call example.
RPC call example finished.
Get number from core1:
Got number: 3
Start normal rpc call example.
RPC call example finished.
.
.
.