MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the clockout demo in the terminal window:

Clock Output Driver Example.
Please choose one output clock.
        A -- SFRO Clock.
        B -- External Clock.
        C -- Low Power Oscillator Clock.
        D -- FFRO Clock.
        E -- Main Clock.
        F -- DSP Main Clock.
        G -- Main System PLL.
        H -- SYSPLL0 AUX0 PLL.
        I -- DSP PLL.
        J -- SYSPLL0 AUX1 PLL.
        K -- AUDIO PLL.

To measure the output clock signal, please use the oscilloscope to probe TP52(P2_29).