Hardware requirements

  • Micro USB cable

  • LPC54018-IoT-Module + Baseboard

  • Personal Computer

Board settings

To make i2c example work, connections needed to be as follows: I2C4 connected to I2C2 SCL P0_29(J27 pin2) –> P0_18(J30 pin6) SDA P0_30(J27 pin1) –> P0_17(J30 pin5) Make sure JP42 2-3 is connected.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J5) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.