Hardware requirements#
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Headphone
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-LINK USB port (J54) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, you can hear the sound from microphone(U66, U67) and the log would be seen on the terminal like:
PDM SAI multi channel edma example started!