Hardware requirements

  • Micro USB cable

  • mimxrt700evk

  • Personal Computer

  • One of the following modules:

    • Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.

Board settings

Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_BOARD). If you want to use Embedded Artists 2EL M.2 Module(Rev-A1), please change the macro to WIFI_IW612_BOARD_MURATA_2EL_M2.

Jumper settings for RT700-EVKC (enables external 5V supply):

remove J2 5-6 connect J2 1-2 connect J45 with external power(controlled by SW4)

Murata Solution Board settings

Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf

The hardware should be reworked according to the hardware rework guide for mimxrt700evk and Murata 2EL M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL.

Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW7 or power off and on the board to run the application.