Hardware requirements#
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings#
Switch the JP45 jumper to the 2-3 configuration and the JP46 jumper to the 2-3 configuration to enable XSPI1 memory access. Switch the SW10 boot mode switch to the 11 XSPI1 flash configuration.
Prepare the Demo#
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the RPMsg-Lite pingpong TZM demo in the terminal window:
Copy CORE1 image to address: 0x2004e000, size: 9952
RPMsg demo starts
Data exchange in secure domain
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 51
Entering normal world now.
Non-secure portion of the application started!
Data exchange in non-secure domain
Primary core received a msg
Message: DATA = 1001
Primary core received a msg
Message: DATA = 1003
Primary core received a msg
Message: DATA = 1005
.
.
.
Primary core received a msg
Message: DATA = 1051
RPMsg demo ends
Note#
This example is currently not supported in MCUXpresso IDE.
TrustZone Application Development in SDK#
Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.
The primary core secure project is stored in <application_name><primary core name><application_name>_s directory. The primary core non-secure project is stored in <application_name><primary core name><application_name>_ns directory.
The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. If IDE allows the two primary core projects in single workspace, the user can also find the project with <application_name>. This project contains both secure and non-secure projects in one workspace (Keil MDK, IAR) and it allows to user easy transition from one to another project.
Project Structure#
The all TrustZone files related to TrustZone are located in trustzone virtual directory. The files are:
tzm_config.c
tzm_config.h
veneer_table.c
veneer_table.h
File tzm_config.c, tzm_config.h#
This file is used by secure project only. It contains one function BOARD_InitTrustZone(), which configures complete TrustZone environment. It includes SAU, MPU’s, AHB secure controller and some TrustZone related registers from System Control Block. This function is called from SystemInitHook() function, it means during system initialization.
File veneer_table.c, veneer_table.h#
This file defines all secure functions (secure entry functions) exported to normal world. This file is located in secure project only. While header file is used by both secure and non-secure projects. The secure entry functions usually contain validation of all input parameters in order to avoid any data leak from secure world.
The files veneer_table.h and <application_name>_s_import_lib.o or <application_name>_s_CMSE_lib.o create the connection between secure and non-secure projects. The library file is generated by linker during compilation of secure project and it is linked to the non-secure project as any other library.
TrustZone application compilation#
As first compile primary core secure project since CMSE library is needed for compilation of non-secure project. After successful compilation of primary core secure project, compile primary core non-secure project.
TrustZone application debugging#
Download both output file into device memory
Start execution of secure project since secure project is going to be executed after device RESET.
If IDE (Keil MDK, IAR) allows to manage download both output files as single download, the primary core secure project is configured to download both secure and non-secure output files so debugging can be fully managed from primary core secure project.
Device header file and secure/non-secure access to the peripherals#
Both secure and non-secure project uses identical device header file. The access to secure and non-secure aliases for all peripherals is managed using compiler macro __ARM_FEATURE_CMSE.
For secure project using <PERIPH_BASE> means access through secure alias (address bit A28=1), using <PERIPH_BASE>_NS means access through non-secure alias(address bit A28=0) For non-secure project using <PERIPH_BASE> means access through non-secure alias (address bit A28=0). The non-secure project doesn’t have access to secure memory or peripherals regions so the secure access is not defined.
J-Link debugger usage#
J-Link V6.71a and above needs to be used in case the J-Link Commander is used for loading individual parts of this application (using loadfile or loadbin commands).