Hardware requirements#
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings#
USART hardware flow control on one board. The USART sends data to itself(loopback), and hardware flow control function is enabled on this example. So please make sure the correct connection for example.
Pin Name Board Location connect to Pin Name Board Location
USART_TX HD2 Pin 4 ---------- USART_RX HD2 pin 3
USART_CTS HD11 Pin 14 ---------- USART_RTS HD11 Pin 8
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the terminal like:
This is USART hardware flow control example on one board.
This example will send data to itself and will use hardware flow control to avoid the overflow.
Please make sure you make the correct line connection. Basically, the connection is:
USART_TX -- USART_RX
USART_RTS -- USART_CTS
Data matched! Transfer successfully.