MCUXpresso SDK Documentation

secure_faults_trdc_s

secure_faults_trdc_s#

Overview#

The Secure Faults demo application demonstrates handling of different secure faults. This application is based on application Hello World. In addition, user can invoke different secure faults by setting testCaseNumber variable (see source code). The following faults can be invoked:

TEST 0: No any secure fault TEST 1: Invalid transition from secure to normal world TEST 2: Invalid entry point from normal to secure world TEST 3: Invalid data access from normal world, example 1 TEST 4: Invalid input parameters in entry function TEST 5: Invalid data access from normal world, example 2

Supported Boards#

EVK9-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Create a directory named ‘tz_bin’ in your work direcory.

  2. Build {app}_s and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_s.bin.

  3. Build {app}_ns and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_ns.bin.

  4. Enter the ‘tz_bin’ directory and execute ‘dd’ command to combin the two files. dd if=sdk2.0-app_ns.bin of=sdk2.0-app_s.bin bs=1 count=ls -l ./sdk2.0-app_ns.bin|awk '{print $5}' seek=843776

  5. Rename sdk2.0-app_s.bin as m33_image.bin, and copy it into imx-mkimage

  6. Build the corresponding flash.bin

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30000000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.
TRDC MBC slavemem:1 Violent access
    domainId        : 0
    Address         : 0x20040000
    Error state     : 2
    Error attribute : 7
    Error type      : 0
    Error port      : 1
TrustZone Application Development in SDK

Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.

The secure project is stored in <application_name><application_name>_s directory. The non-secure project is stored in <application_name><application_name>_ns directory.

The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. If IDE allows the two projects in single workspace, the user can also find the project with <application_name>. This project contains both secure and non-secure projects in one workspace (armgcc, IAR) and it allows to user easy transition from one to another project.

Project Structure

The all TrustZone files related to TrustZone are located in trustzone virtual directory. The files are:

  • tzm_config.c

  • tzm_config.h

  • veneer_table.c

  • veneer_table.h

File tzm_config.c, tzm_config.h

This file is used by secure project only. It contains one function BOARD_InitTrustZone(), which configures complete TrustZone environment. It includes SAU, TRDC and some TrustZone related registers from System Control Block. This function is called from SystemInitHook() function, it means during system initialization.

File veneer_table.c, veneer_table.h

This file defines all secure functions (secure entry functions) exported to normal world. This file is located in secure project only. While header file is used by both secure and non-secure projects. The secure entry functions usually contain validation of all input parameters in order to avoid any data leak from secure world.

The files veneer_table.h and <application_name>_s_import_lib.o or <application_name>_s_CMSE_lib.o create the connection between secure and non-secure projects. The library file is generated by linker during compilation of secure project and it is linked to the non-secure project as any other library.

TrustZone application compilation

Please compile secure project firstly since CMSE library is needed for compilation of non-secure project. After successful compilation of secure project, compile non-secure project.

EVK-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Create a directory named ‘tz_bin’ in your work direcory.

  2. Build {app}_s and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_s.bin.

  3. Build {app}_ns and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_ns.bin.

  4. Enter the ‘tz_bin’ directory and execute ‘dd’ command to combin the two files. dd if=sdk2.0-app_ns.bin of=sdk2.0-app_s.bin bs=1 count=ls -l ./sdk2.0-app_ns.bin|awk '{print $5}' seek=843776

  5. Rename sdk2.0-app_s.bin as m33_image.bin, and copy it into imx-mkimage

  6. Build the corresponding flash.bin

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30000000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.
TRDC MBC slavemem:1 Violent access
    domainId        : 0
    Address         : 0x20040000
    Error state     : 2
    Error attribute : 7
    Error type      : 0
    Error port      : 1
TrustZone Application Development in SDK

Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.

The secure project is stored in <application_name><application_name>_s directory. The non-secure project is stored in <application_name><application_name>_ns directory.

The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. If IDE allows the two projects in single workspace, the user can also find the project with <application_name>. This project contains both secure and non-secure projects in one workspace (armgcc, IAR) and it allows to user easy transition from one to another project.

Project Structure

The all TrustZone files related to TrustZone are located in trustzone virtual directory. The files are:

  • tzm_config.c

  • tzm_config.h

  • veneer_table.c

  • veneer_table.h

File tzm_config.c, tzm_config.h

This file is used by secure project only. It contains one function BOARD_InitTrustZone(), which configures complete TrustZone environment. It includes SAU, TRDC and some TrustZone related registers from System Control Block. This function is called from SystemInitHook() function, it means during system initialization.

File veneer_table.c, veneer_table.h

This file defines all secure functions (secure entry functions) exported to normal world. This file is located in secure project only. While header file is used by both secure and non-secure projects. The secure entry functions usually contain validation of all input parameters in order to avoid any data leak from secure world.

The files veneer_table.h and <application_name>_s_import_lib.o or <application_name>_s_CMSE_lib.o create the connection between secure and non-secure projects. The library file is generated by linker during compilation of secure project and it is linked to the non-secure project as any other library.

TrustZone application compilation

Please compile secure project firstly since CMSE library is needed for compilation of non-secure project. After successful compilation of secure project, compile non-secure project.

MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for MCIMX93AUTO-EVK.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Build secure binary and non-secure binary. For example (if west build is used), west build -p -b mcimx93autoevk examples/trustzone_examples/secure_faults_trdc_s -Dcore_id=cm33 -d secure_faults_trdc_s west build -p -b mcimx93autoevk examples/trustzone_examples/secure_faults_trdc_ns -Dcore_id=cm33 -d secure_faults_trdc_ns

  2. Create m33_image.bin dd if=secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin of=secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin bs=1 count=ls -l secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin | awk '{print $5}' seek=65536 Rename secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin to m33_image.bin

  3. Copy m33_image.bin into imx-mkimage to make low power boot flash.bin.

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30003000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.
MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for MCIMX93-EVK.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Build secure binary and non-secure binary. For example (if west build is used), west build -p -b mcimx93evk examples/trustzone_examples/secure_faults_trdc_s -Dcore_id=cm33 -d secure_faults_trdc_s west build -p -b mcimx93evk examples/trustzone_examples/secure_faults_trdc_ns -Dcore_id=cm33 -d secure_faults_trdc_ns

  2. Create m33_image.bin dd if=secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin of=secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin bs=1 count=ls -l secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin | awk '{print $5}' seek=65536 Rename secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin to m33_image.bin

  3. Copy m33_image.bin into imx-mkimage to make low power boot flash.bin.

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30003000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.
MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93W-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for MCIMX93W-EVK.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Build secure binary and non-secure binary. For example (if west build is used), west build -p -b mcimx93wevk examples/trustzone_examples/secure_faults_trdc_s -Dcore_id=cm33 -d secure_faults_trdc_s west build -p -b mcimx93wevk examples/trustzone_examples/secure_faults_trdc_ns -Dcore_id=cm33 -d secure_faults_trdc_ns

  2. Create m33_image.bin dd if=secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin of=secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin bs=1 count=ls -l secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin | awk '{print $5}' seek=65536 Rename secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin to m33_image.bin

  3. Copy m33_image.bin into imx-mkimage to make low power boot flash.bin.

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30003000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.
MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • MCIMX93-QSB board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for MCIMX93-QSB.pdf’ to make and download flash.bin.

  5. Press the reset button on your board.

How to get flash.bin of TrustZone examples:
  1. Build secure binary and non-secure binary. For example (if west build is used), west build -p -b mcimx93qsb examples/trustzone_examples/secure_faults_trdc_s -Dcore_id=cm33 -d secure_faults_trdc_s west build -p -b mcimx93qsb examples/trustzone_examples/secure_faults_trdc_ns -Dcore_id=cm33 -d secure_faults_trdc_ns

  2. Create m33_image.bin dd if=secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin of=secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin bs=1 count=ls -l secure_faults_trdc_ns/secure_faults_trdc_ns_cm33.bin | awk '{print $5}' seek=65536 Rename secure_faults_trdc_s/secure_faults_trdc_s_cm33.bin to m33_image.bin

  3. Copy m33_image.bin into imx-mkimage to make low power boot flash.bin.

Running the demo

The log below shows the output of the secure_faults demo in the terminal window:

Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!

Change testCaseNumber value in secure_faults_s project to triger different secure error. The available testCaseNumber values are defined in veneer_table.h as macro, #define FAULT_NONE 0 #define FAULT_INV_S_TO_NS_TRANS 1 #define FAULT_INV_S_ENTRY 2 #define FAULT_INV_NS_DATA_ACCESS 3 #define FAULT_INV_INPUT_PARAMS 4 #define FAULT_INV_NS_DATA2_ACCESS 5 In case some secure error is raised, the information about error will be printed in the terminal window.

With testCaseNumber = FAULT_INV_S_TO_NS_TRANS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.

Entering HardFault interrupt!
SAU->SFSR:INVTRAN fault: Invalid transition from secure to normal world.

With testCaseNumber = FAULT_INV_S_ENTRY, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:INVEP fault: Invalid entry point to secure world.

With testCaseNumber = FAULT_INV_NS_DATA_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SAU->SFSR:AUVIOL fault: SAU violation. Access to secure memory from normal world.
Address that caused SAU violation is 0x30003000.

With testCaseNumber = FAULT_INV_INPUT_PARAMS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!
Input data error: String is not located in normal world!

With testCaseNumber = FAULT_INV_NS_DATA2_ACCESS, the below log will be shown in the terminal:

Hello from secure world!
Entering normal world.
Welcome in normal world!

Entering HardFault interrupt!
SCB->BFSR:PRECISERR fault: Precise data access error.
Address that caused secure bus violation is 0x20040000.