Hardware Rework Guide for MIMXRT595-EVK and AW-AM510MA#
This section is a brief hardware rework guidance of the EdgeFast Bluetooth PAL on the NXP i.MX MIMXRT595-EVK board and AW-AM510MA. The AW-AM510MA user guide is available here. The hardware rework has one part:
Debug console serial rework
Hardware rework#
Debug console serial rework:
No special rework is required, except the following to enable the debug port.
Connect J39 with external power.
Connect JP4 1-2.
J27 1 — TX of USB to serial converter.
J27 2 — RX of USB to serial converter.

Parent topic:Hardware Rework Guide for MIMXRT595-EVK and AW-AM510MA