MCUXpresso SDK Documentation

Hardware Rework Guide for MIMXRT595-EVK and Murata M.2 Module

Contents

Hardware Rework Guide for MIMXRT595-EVK and Murata M.2 Module#

This section is a brief hardware rework guidance of the EdgeFast Bluetooth PAL on the NXP i.MX MIMXRT595-EVK board and the Murata’s 1XK, 1ZM, 2EL or 2LL solution - direct M.2 connection to Embedded Artists EAR00385 (1XK), EAR00364 (1ZM), Rev-A1 (2EL) or EAR00500 (2LL) M.2 modules.

The hardware rework has one part:

  • Debug console serial rework

Hardware rework#

Debug console serial rework:

No special rework is required, except the following to enable the debug port.

  • JP4 1-2.

  • J27 1 - TX of USB to serial converter

  • J27 2 - RX of USB to serial converter

Parent topic:Hardware Rework Guide for MIMXRT595-EVK and Murata M.2 Module