MCUXpressoSDK EdgeFast Bluetooth Protocol Abstraction# Table of Contents Introduction Stack API Reference Overview Folder structure Architecture Features Bluetooth features Toolchain support RTOS support Examples list Hardware Reference boards list Dual-chip wireless module list Demo Run a demo application using IAR Open an IAR example Build an IAR example Run an IAR example Run a demo application using MCUXpresso IDE Open an MCUXpresso IDE example Build an MCUXpresso IDE example Run an MCUXpresso IDE example Run a demo application using MDK Open an MDK project Build an MDK example Run an MDK example Run a demo application using Arm GCC Setup tool chains Build a GCC example Run a GCC example Download Linker Layer firmware from the reference board Change board-specific parameters Change HCI UART parameters Change USB Host stack parameters Known issues Notes EdgeFast BT PAL configuration documentation